8536IB1905EN-05

Motor Two Speeds Two Directions - SIL Stop, W. Cat 3/4

This function block is used to manage a two speed motor in two directions (forward and reverse) with Stop Category 0 or Stop Category 1 function compliance for Wiring Category 3 and Category 4.*

MotorTwoSpeedsTwoDirectionsSILStopCat3and4 Function Block

Modbus TCP Inputs

Input Name Address Starting Bit Size (Bits)
Run Forward High 8501 0 1
Run Reverse High 8501 1 1
Trip Reset 8501 3 1
Run Forward Low 8501 6 1
Run Reverse Low 8501 7 1

Modbus TCP Outputs

Output Name Address Starting Bit Size (Bits)
Thermal Overload Time To Reset 450 0 16
Protection Trip Message 1 452 0 16
Protection Trip Message 2 453 0 16
Protection Alarm Message 1 461 0 16
Protection Alarm Message 2 462 0 16
IRMS Average 500 0 32
Thermal Overload Time To Trip 511 0 16
Ready 3201 0 1
Tripped 3201 2 1
Alarm 3201 3 1
Run Forward Low Status 3201 5 1
Run Forward High Status 3201 6 1
Load Running 3201 8 1
Ready To Reset 3201 9 1
Run Reverse Low Status 3201 12 1
Run Reverse High Status 3201 13 1
Load Starting 3201 15 1
Asset Alarm 3202 3 1
Upstream Voltage Present 1 3202 12 1
Upstream Voltage Present 2 3202 13 1
Upstream Voltage Present 3 3202 14 1
Upstream Voltage Present 4 3202 15 1
Motor Thermal Capacity Used 9630 0 8
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?