8536IB1905EN-05

Using Multiple TeSys™ island Devices in a Single Programming Tool

The EDS file export output is a file specific for the configured island. It contains information that is unique for the avatars and devices, and the order you chose. If you work with multiple islands on your PC or programming environment, you will have multiple EDS files. Generally, a programming tool will not allow conflicts in the product name or revision of multiple imported devices. For example, you cannot import two different EDS files for TeSyS™ island revision 1.1. To work around this and work with multiple island configurations (each island imported as a device in the programming tool), it is recommended that you edit the MinRev and ProdName in the EDS file with either a text editor or EZ-EDS software as shown below.

EZ-EDS Generated Electronic Data Sheet

EZ-EDS TeSys island EDS File Export

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?