Client Considerations

There are multiple options regarding how ArcFM Mobile and the data it uses are deployed to client devices. These options fall under three categories:

  • App deployment

  • Map data deployment

  • Map data usage

You also have the opportunity to set a specific spatial reference, which otherwise defaults to WGS 1984 Web Mercator (EPSG 3857/Esri WKID 102100). Spatial Reference can be set in Solution Center.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.