Markup Considerations

IMPORTANT: The customer-hosted Markup Service option is only available for existing ArcFM Mobile implementations already using this option. All other implementations must use the SE-hosted Markup Service.
  1. ArcFM requires configuration of the ArcFM Markup Service to enable markups. For system requirements, refer to GIS – Supported Versions – ArcFM Mobile Services, Portal, and Tools on myArcFM.

  2. Markups require a dataset with a storage type of ST_GEOMETRY or SDO_GEOMETRY for Oracle databases or GEOMETRY for SQL Server databases. If your geodatabase uses either SDELOB or SDEBINARY, you must either enable a new configuration keyword on your geodatabase, or you will need to migrate your storage type. For more information about configuration keywords, refer to Esri’s Configuration Keywords for Enterprise Geodatabases article.

  3. Will you use the default markup palette provided with ArcFM? If so, refer to ArcFM Markup Sample Data on myArcFM for installation steps.

  4. If you create custom markup palettes, palette design and configuration are required. Refer to Markup Configuration.

  5. Cloud services deployment requires HTTPS, so ensure that you have it set up before considering this type of deployment.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?