Sideload Data to Windows Devices

The methods to sideload data are dependent upon the installation method you chose after reviewing the Client Considerations topic. There are two things you should know before reading further:

  • If you are not using the shared data approach, all downloaded information is saved in one location, per user, on the device. Only the user who downloaded the data has access to it; additional users need to perform a download of the same data to have access to it.

  • If you are using shared data, all downloaded information is saved in a location (different from the location above) that all users of the device can access.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.