Configure Operational Maps in ArcMap

Prior to creating an operational map in ArcMap, Global IDs need to be added to use your feature service locally in a client application and are required even for one-way replication.

IMPORTANT: Your published operational map broadcasts its native map units, i.e., meters or feet. When a user loads an operational map, ArcFM Mobile checks that map's spatial reference and switches the map unit used for the measure tool. When preparing operational maps, it’s important to use a spatial reference that’s appropriate for the system of units most commonly used in your region.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?