Option 2: Customer-Managed Markup Service

A customer-managed Markup Service deployment involves installation and configuration of a web service on a separate server managed by your organization. Follow the steps in this section to help you with the deployment.

IMPORTANT:
  • The customer-managed Markup Service option is only available for existing ArcFM Mobile implementations already using this option.

  • If Portal for ArcGIS is behind a proxy, you need to have Hybrid Connection Manager installed and configured. Refer to the HCM configuration steps in Schneider Electric-Managed Markup Service.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?