Configure Operational Maps

Operational maps contain the GIS features with which users interact in ArcFM Mobile. Operational maps must be dynamic map services and need to be visible to mobile devices through a virtual private network (VPN) or some other means. Feature services are required by ArcFM Mobile for both online and offline viewing/querying because the feature service exposes more querying capabilities. To alleviate potential heavy server processing load and network traffic, the app utilizes the map service to retrieve information for panning and zooming functions.

The following Esri links provide some useful information:

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.