Set Permissions on the Replicas Folder

If you have chosen to save your replicas on a computer other than the one running the Sync Service, you need to provide permissions to the machine running the Sync Service at that location.

  1. In Windows File Explorer, right-click the folder that contains your replicas and click Properties.
  2. In the resulting dialog, click the Sharing tab and then click Advanced Sharing.
  3. Check the box next to Share this folder, then click Permissions.
  4. Click Object Types and check the box next to Computers.
  5. For the object name, enter the name of the server running the Sync Service.

  6. Click OK.
  7. After your computer is added to the list of groups and usernames, be sure to grant both Change and Read permissions to the computer.
  8. Click OK.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.