Configure Operational Maps in ArcGIS Pro

To create an operational map, you must first publish a feature service. Prior to this, you must have:

  • An established database

  • An existing or staged Utility Network

  • An applied Asset Package

The steps in this section include how to publish a feature service.

IMPORTANT:
  • Definition queries and hidden fields set using the visible field property are not supported. Analyzer errors are returned if these exist. Refer to Esri’s Fields view article plus the Publish and consume services article for more information about layer dependence.

  • Due to ArcGIS Pro’s inconsistency with refreshing between changes, if you receive an error saying Tools failed to open, remember to frequently save, exit, then re-launch the app as you progress through the steps below.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.