Configure Data

Similar to operational map and basemap configuration for online viewing, configuration of replicas and tile packages for offline viewing requires use of ArcGIS tools and Solution Center. A replica is an offline operational map and a tile package is an offline basemap.

NOTE: If you have maps that use custom fonts for symbols, those font files need to be manually deployed to all mobile devices. Refer to the following helpful topics:

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.