Configure Markup Service

Publishes only in Mobile config

The ArcFM Markup Service is required for markups captured in ArcFM Mobile to be synced back to the enterprise.

IMPORTANT: The customer-managed Markup Service option is only available for existing ArcFM Mobile implementations already using this option.

Option 1: SE-managed Markup Service

With this default option, Schneider Electric manages the scaling and upgrades of the Markup Service, and no additional customer-managed servers are required.

Option 2: Customer-managed Markup Service

With this option, you must provide a server for the Markup Service. The responsibility for scaling, maintenance, and upgrades of the server plus the Markup Service lies in your organization’s hands.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?