Configure Layer Settings

Publishes in Mobile config

Depending on your version of ArcMap, layer settings may not be displayed in ArcMap the same as they are in Mobile. If layers don't appear as expected in ArcMap, follow the instructions in these topics to correct the settings.

Edit Dimension Line Label Properties

Publishes in Mobile config

Follow these steps to edit label properties for a dimension line:

  1. Open the Properties dialog for the layer.
  2. Click the Labels tab.
  3. To view labels for this layer, check Label features in this layer.
  4. Edit any other label characteristics including symbology and label placement.
  5. Click OK.

Edit Highlight Properties

Publishes in Mobile config

Follow the steps below to edit the properties for a layer that has a transparency value:

  1. Open the Properties dialog for the layer.
  2. Click the Display tab.
  3. Type the desired transparency in the Transparent field.
  4. Click OK.

Once you're satisfied with the configuration for markups, save it to an MXD file or to a Stored Display to make the viewing of future ArcMap markup sessions more convenient. If you save to an MXD, and you want other users to have access to it, save it to a shared location.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?