Operational Maps in ArcGIS Pro

For users to take their operational data offline, you need to create runtime databases (replicas) on a mobile device from sync-enabled feature services via ArcGIS Server. You should have already created an operational map during online viewer configuration, but if you need to create additional operational maps, refer to Configure Operational Maps for further details. Feature services for offline operation have additional requirements. Refer to Esri’s Prepare data for offline use to establish an awareness of the data requirements for sync capability on feature services.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.