Configure As-Built Markups for Operational Maps

Publishes in Mobile config Construction As-Builting Configuration section.

The Markup tab provides a list of markup types that are available for a selected operational map. You can configure each markup type to use the default markup palette (defined on the Markup Types tab), or you can override those settings.

  • For each markup type in the list, leave the Use Default Palette toggle enabled if you want to use the default markup palette, as defined on the Markup Types tab.

  • To completely disable the associated markup type on the selected map, toggle Use Default Palette off, then toggle Disable on.

  • To override the setting on the Markup Types tab for the selected markup type, toggle Use Default Palette off then provide a URL to the feature service that defines the markup palette for this type.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?