Replicas

Replicas are copies of operational maps that mobile users can download and interact with on their devices. Deltas contain incremental changes to an operational map that have occurred since a replica was created. ArcFM Mobile automatically downloads deltas to a mobile device when they become available and the device has connectivity. Consolidating deltas into the base replica allows any newly provisioned mobile devices to download just the replica file, rather than having to download the replica and all the deltas associated with it.

Replicas can only be created for operational maps that are sync-enabled. Refer to Feature Service Publishing for details.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.