Enable Roles and Features

Certain server and web roles and features need enabled on whichever server version you are using to host the Sync Service. Consult the help documentation for your operating system if you are unsure of how to manage roles and features.

Ensure the following roles and features are enabled on your server (Windows Server 2012 R2 and later):

Server Roles

  • Web Server IIS

Web Server Roles

  • .NET Extensibility 4.5

  • Application Initialization

  • ASP.NET 4.5

Features

  • ASP.NET 4.5

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.