ArcFM Solution Center Install

Numerous configuration settings must be made in Solution Center, our seamless application for configuring the entire ArcFM XI series.

Before installing Solution Center, you need to download, install, and run the ArcFM Connectivity Evaluator tool, which is a separate application from Solution Center. Its core function is to test and verify connectivity to ArcFM services and, depending on the application, connectivity to Azure Service Bus.

Both the ACE tool installer and the Solution Center installer are available on the myArcFM Solution Center product page.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.