DOCA0257ZH-CN-01

HMI 通讯中断

描述

HMI 通讯中断功能:

  • 通讯建立,即检测 LTMT main unitHMI(通过连接 HMI 端口连接)之间的通讯中断。

  • 根据功能设置生成报警或脱扣操作。

参数设置

Parameter

Range

Default value

Function

  • Disable

  • Alarm

  • Trip

  • Alarm + Trip

Disable

Time Delay

0.1 – 6000.0 s in step of 0.1 s

1 s

Reset Mode

  • Reset key

  • DI

  • Communication

  • Auto

DI + Reset Key

Auto Reset Delay

0.0 – 6000.0 s in step of 0.1 s

0 s

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?