过频
描述
Over Frequency 保护功能产生以下信号:
-
报警:测得的频率高于报警级别。
-
脱扣:在指定时间延迟内,测得的频率高于脱扣级别。
参数设置
Over Frequency 保护功能具有以下可配置的设置:
|
Parameter |
Setting range |
Default value |
|---|---|---|
|
Function |
|
Disable |
|
Trip Level |
100–110% of nominal frequency in step of 1% |
105% of nominal frequency |
|
Time Delay |
0.1–6000.0 s in step of 0.1 s |
0.1 s |
|
Alarm Level |
100–110% of nominal frequency in step of 1% |
105% of nominal frequency |
|
Reset Mode |
|
DI + Reset Key |
|
Auto-Reset Delay (applicable only if Reset mode is Auto) |
0.0–6000.0 s in step of 0.1 s |
0 s |