EIO0000004200.07

Replacing the Installation Gasket

Introduction

The installation gasket provides protection against dust and moisture. The gasket must be inserted correctly into the groove for moisture resistance for the Panel Type.

NOTICE
GASKET AGING
  • Inspect the gasket periodically as required by your operating environment.
  • Replace the gasket at least once a year, or as soon as scratches or dirt become visible.
Failure to follow these instructions can result in equipment damage.
NOTICE
EQUIPMENT DAMAGE
Be careful not to stretch the gasket unnecessarily.
Failure to follow these instructions can result in equipment damage.

Installing the Installation Gasket

  1. Place the Panel Type on a flat, level surface, with the display face pointing down.
  2. Remove the gasket from the Panel Type.
  3. Attach the new gasket to the Panel Type. Insert the protrusions from the four corners of the gasket into the corresponding holes in the corners of the Panel Type.
    Depending on your model, there may be additional protrusions. In the following, refer to the figure on the right and insert the protrusions accordingly.
    NOTE: When using a tool to insert the gasket, make sure the tool does not catch the rubber gasket and cause a tear.
    1. Installation gasket

    2. Protruding point

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.