EIO0000004200.07

Wall mounting when installing PCI/PCIe slot

When the PCI/PCIe slot is connected to Advanced Box, wall mounting requires an optional flat/wall mount adapter.

Flat/wall mount adapter: HMIYP6ADFMA

Installation procedure

  1. Use the screws for the flat/wall mount adapter to attach it to the product.
    (Attach on both the top and bottom of the product.)
    NOTE:
  2. Install the product to the panel or wall with M4 screws (4 pieces).
    NOTE:
    • The necessary torque is 1.5 N•m (13.3 lb-in).

    • To prevent abnormally high temperatures from occurring inside the product, mount the product completely vertically or horizontally.

    • When mounting the product vertically, the interface side (the bottom of the product) must be facing downward.

    • When mounting the product horizontally, the heat sink must be facing upward.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.