EIO0000004200.07

Changing to RAID Mode

Use Intel® OptaneTM Memory and Storage Management to change from AHCI mode to RAID mode. The procedure for getting this tool varies depending on the OS Base version. Set up by referring to the following.

To protect against data corruption or changes to AHCI mode, before changing to RAID mode, prepare recovery media. Purchase the Recovery USB accessory (HMIYP6RUSW10 or HMIYP6RUSW1021), or use a compatible USB memory device to create a backup USB.

NOTE: The optional recovery USB recovers the operating system only. If you require backup in addition to recovery of the operating system, refer to System Backup.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.