EIO0000004200.07

Installing the Display Module on the Box Module

NOTICE
BROKEN ENCLOSURE
Do not exert more torque than the amount specified.
Failure to follow these instructions can result in equipment damage.
  1. Place the Display Module on a clean and level surface with the screen facing down.
  2. Cover the Box Module so that its outline fits in the appropriate guidelines and you can enter the mounting pins through the holes.
    1. Advanced Box guideline

    2. Standard Box guideline

    3. Installation pins

  3. Tighten the M4 screws (4 pieces) to attach the Box Module.
    NOTE: The necessary torque is 0.7 N•m (6.2 lb-in).
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.