EIO0000004200.07

RAID Rebuild with Intel® Rapid Storage Technology

To rebuild RAID, due to reasons such as disk replacement, follow the procedure below.
NOTE:
  • When replacing a disk, use the same disk product as before. Refer to Accessories.

  • For information, refer to the Intel® Rapid Storage Technology online help.

  1. Select Manage, then select Rebuild to another disk.
  2. Select the disk, then click Rebuild.
  3. Rebuild begins and the progress indicator is displayed. When rebuild is complete, the progress indicator disappears.
  4. Confirm that the progress indicator has disappeared, and restart this product.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.