EIO0000004200.07

TPM

This product comes equipped with the TPM 2.0 module.

Enable or disable TPM in accordance with the laws, regulations, and standards of each country.

TPM is enabled by default.

NOTE: Enable BitLocker to make your system more secure.

TPM Setup Process

  1. Turn on the product.
  2. To disable TPM, press [CTRL]+[D]; to enable TPM, press [CTRL]+[E].
  3. After the setting is updated, the boot screen displays either TPM Disabled or TPM Enabled.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.