EIO0000004200.07

DIMM Installation

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
  • Remove all power from the device before removing any covers or elements of the system, and prior to installing or removing any accessories, hardware, or cables.
  • Unplug the power cable from both this product and the power supply prior to installing or removing the product.
  • Always use a properly rated voltage sensing device to confirm power is off where and when indicated.
  • Replace and secure all covers or elements of the system before applying power to this product.
  • Use only the specified voltage when operating this product. The DC model is designed to use 24 Vdc, and the AC model is designed to use 100 to 240 Vac. Always check whether your device is DC or AC powered before applying power.
Failure to follow these instructions will result in death or serious injury.
CAUTION
MEMORY MODULE DAMAGE AND DATA LOSS
  • Remove all power before making any contact with an installed memory module.
  • Use only our optional memory modules for this product.
  • Confirm the memory module is correctly oriented before insertion.
  • Do not bend, drop, or strike the memory module.
  • Do not touch inside the memory module or its connectors.
  • Do not disassemble or modify the memory module.
  • Keep the memory module dry.
Failure to follow these instructions can result in injury or equipment damage.
NOTICE
ELECTROSTATIC DISCHARGE
Take the necessary protective measures against electrostatic discharge before attempting to remove the cover.
Failure to follow these instructions can result in equipment damage.
NOTICE
BROKEN ENCLOSURE
Do not exert more torque than the amount specified.
Failure to follow these instructions can result in equipment damage.
  1. Disconnect the power supply from the Box Module.
  2. Touch the housing or ground connection (not the power supply) to discharge any electrostatic charge from your body.
  3. Remove 5 screws of the maintenance hatch cover and slide the cover to remove.
  4. As shown below, insert the DIMM module diagonally, then push from above.
  5. Replace the maintenance hatch cover and tighten the screws.
    NOTE: The necessary torque is 0.3 N•m (2.7 lb-in).
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.