EIO0000004200.07

HDD/SSD Installation

You can install 2 HDD or SSD to the Advanced Box, and 1 HDD or SSD to the Standard Box.

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
  • Remove all power from the device before removing any covers or elements of the system, and prior to installing or removing any accessories, hardware, or cables.
  • Unplug the power cable from both this product and the power supply prior to installing or removing the product.
  • Always use a properly rated voltage sensing device to confirm power is off where and when indicated.
  • Replace and secure all covers or elements of the system before applying power to this product.
  • Use only the specified voltage when operating this product. The DC model is designed to use 24 Vdc, and the AC model is designed to use 100 to 240 Vac. Always check whether your device is DC or AC powered before applying power.
Failure to follow these instructions will result in death or serious injury.
CAUTION
STORAGE DEVICE DAMAGE AND DATA LOSS
  • Remove all power before making any contact with an installed storage device.
  • Use only our optional storage devices for this product.
  • Make sure you regularly back up the data.
  • Confirm the storage device is correctly oriented before insertion.
  • Do not bend, drop, or strike the storage device.
  • Do not touch the storage device connectors.
  • Do not disassemble or modify the storage device.
  • Keep the storage device dry.
Failure to follow these instructions can result in injury or equipment damage.
CAUTION
EXCESSIVE VIBRATION
Protect the HDD from vibration and impact when installing or removing it.
Failure to follow these instructions can result in injury or equipment damage.
NOTICE
ELECTROSTATIC DISCHARGE
Take the necessary protective measures against electrostatic discharge before attempting to remove the cover.
Failure to follow these instructions can result in equipment damage.
NOTICE
BROKEN ENCLOSURE
Do not exert more torque than the amount specified.
Failure to follow these instructions can result in equipment damage.
  1. Disconnect the power supply from the Box Module.
  2. Touch the housing or ground connection (not the power supply) to discharge any electrostatic charge from your body.
  3. Remove 5 screws of the maintenance hatch cover and slide the cover to remove.
  4. Insert the HDD or SSD into the slot.
    Advanced Box: 2 slots (refer to the following)
    Standard Box: 1 slot
    1. Disk 2

    2. Disk 1

  5. When removing the HDD or SSD, pull the tab.

    A. Tab

  6. Replace the maintenance hatch cover and tighten the screws.
    NOTE: The necessary torque is 0.3 N•m (2.7 lb-in).
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.