EIO0000004200.07

Model Names

Box Module and Panel Type are referred to as follows.

Panel Type is an all-in-one model in which the Box Module and Display Module are already connected.

  Box Module Panel Type
Core i7 Advanced Box ●●-inch/●●-inch Wide Advanced Model
Core i5
Celeron
Core i3 Standard Box ●●-inch/●●-inch Wide Standard Model
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.