EIO0000004200.07

Audio (Mic-IN, Line-IN, Line-OUT)

Specifications

  1. Line-OUT

  2. Line-IN

  3. Mic-IN

Product number HMIYP6MPAU
Connector 3.5 mm stereo mini jack x 3 (Mic-IN, Line-IN, Line-OUT)
Standard USB Audio Class Rev.1.0 and 2.0
Channels 2-channels / port
Supported Playback / Recording Sampling rate 8/16/22/24/32/44.1/48/96/176.4/192/384 kHz (16/24/32 bit)
WARNING
UNINTENDED EQUIPMENT OPERATION
Do not use this equipment for the critical alarms.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.