EIO0000004200.07

Ethernet (GbE IEEE1588)

Specifications

NOTE: Install the latest version of the driver before using this interface. You can download the latest driver from our website.
www.se.com/ww/en/download
Product number HMIYP6MPETH
Connector Modular jack (RJ-45) x 1
Standard IEEE1588, 10 BASE-T/100 BASE-TX/1000 BASE-T, Wake-on-LAN (WOL) supported*1
Maximum communication distance 100 m (328.1 ft)

*1 When the status is S4 (hybrid shutdown), Wake-on-LAN is unavailable.

CAUTION
LOSS OF COMMUNICATION
  • Do not put excessive stress on the communication ports of all connections.
  • Securely attach communication cables to the panel wall or cabinet.
Failure to follow these instructions can result in injury or equipment damage.

LED Indications

Color Indicator Description
Green (Active) ON Data transmission is available
Flashing Data transmission in progress
OFF No connection or error
Green (Link) ON Data transmission is available.
OFF No data transmission
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.