EIO0000004200.07

OS Base version 3.0 or later

  1. Save the file C:\Program Files\Schneider Electric\Utilities\RAID\Intel(R) Optane Memory and Storage Management\rst_pv_xxxxxxxxxxxxxxxxxx.zip to the root of C drive (C:\rst_pv_xxxxxxxxxxxxxxxxxxxxxxxxx.zip, where xxx is the version information).
  2. Extract the files from the compressed file in the root of C drive.
  3. Run SetupRST.exe.
NOTE: After execution, deleting the downloaded and extracted files is recommended.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.