EIO0000004200.07

Touch Panel

  12-inch, 15-inch 10-inch Wide, 12-inch Wide, 15-inch Wide, 19-inch Wide, 22-inch Wide
Touch panel type Resistive film (analog) Projected capacitive with optimized noise filter
Touch points Multi-touch (two-point touch) Multi-touch (two-point touch)
Touch panel service life 1 million times or more 50 million times or more
Touch mode Not applicable

Standard mode, water detection mode, glove mode

NOTE: For details, refer to Touch Mode.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.