EIO0000004200.07

RAID Rebuild with Intel® OptaneTM Memory and Storage Management

To rebuild RAID, due to reasons such as disk replacement, follow the procedure below.
NOTE:
  • When replacing a disk, use the same disk product as before. Refer to Accessories.

  • For information, refer to the Intel® OptaneTM Memory and Storage Management online help.

  1. Select Manage, then select the button that appears on the notation for the replaced disk.
  2. Select Rebuild to another disk.
  3. Select Rebuild.
  4. Rebuild begins and the progress indicator is displayed. When rebuild is complete, the progress indicator disappears.
  5. Confirm that the progress indicator has disappeared, and restart this product.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.