EIO0000004200.07

OS Base version 2.0 or earlier

  1. Download the Intel® OptaneTM Memory and Storage Management from the following URL.
    www.se.com/ww/en/download
  2. Save the downloaded file in the root of C drive (C:\rst_pv_xxxxxxxxxxxxxxxxxxxxxxxxxx.zip, where xxx is the version information).
  3. Extract the files from the downloaded file in the root of C drive.
  4. Run SetupRST.exe.
NOTE: After execution, deleting the downloaded and extracted files is recommended.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.