EIO0000004200.07

Edit

You can use this function to customize the icons displayed on the Launcher. You can also add any application to the display.

  1. You can change the name of the icon.

  2. You can change the application displayed. Click to display a screen where you can select the application’s exe file. Select the exe file of the application you want to display.

  3. Click this mark to remove the icon.

  4. Add the application displayed. Click to display a screen where you can select the application’s exe file. Select the exe file of the application you want to display.

  5. Returns the icon display to the factory default settings.

  6. This button releases Edit mode.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.