EIO0000004200.07

Connecting the AC Power Cord

AC Power Connector: Spring Clamp Terminal Blocks

Connection Wire
L Live
N Neutral

How to Connect the AC Power Cord

  1. Loosen the screw on the product’s PE terminal, connect the grounding wire, and tighten the screw.
    NOTE:
    • The necessary torque is 1.5 N•m (13.3 lb-in).

    • If the wire is not connected to the PE terminal properly, touch may not respond normally.

    1. Advanced Box

    2. Standard Box

    3. This mark indicates that you must use copper wire rated for 75 °C (167 °F) or higher.

  2. Confirm the power cord is not connected to the power supply.
  3. Crimp a pin terminal properly to the end of each power cable wire.
  4. Push the opening button with a small and flat screwdriver to open the desired pin hole.
  5. Insert each power cord wire into its corresponding hole. Release the opening button to clamp the wire in place.
    NOTE:
    • When using stranded wire, do not short with neighboring wires.

    • When connecting with stranded wires, do not solder the stranded wires.

    1. Power cord

    2. Black

    3. White

    4. Opening button

    5. Screw

  6. After inserting all two power cord wires, insert the AC power connector into the power connector on this product.
  7. Affix the screws on both sides of the connector.
    NOTE: The necessary torque is 0.3 N•m (2.7 lb-in).
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.