EIO0000004200.07

EtherCAT Driver and Firmware Installation

  1. Download the EtherCAT Utility/Driver file (PFXPHMIP6_EtherCAT_********.zip) from our site.
    www.se.com/ww/en/download
  2. Install the driver. Unzip the downloaded file, select Driver_&_Toolkit > Device Driver (NXDRV-WIN) > Installation, and run cifX Device Driver Setup. Install following the on-screen instructions.
    NOTE: The file storage location may change depending on the version.
  3. Next, install SYCON.net. Select Software_&_Tools > Configuration_Software > SYCON.net > SYCON.net, and run SYCONnet netX Setup. Install following the on-screen instructions.
    NOTE: The file storage location may change depending on the version.
  4. From the Windows Start menu, select SYCON.net.
  5. The login screen is displayed. Click OK.
  6. In the right-pane of the displayed screen, open EtherCAT > Master, and drag CIFX RE/ECM to the netDevice line.
  7. Double-click the displayed icon.
  8. The following screen appears. Select Settings > Driver. Select the CIFX Device Driver and netX Driver check boxes, and select Apply.
  9. Select Settings > Device Assignment. Confirm Device Selection is set to all, and click Scan. In the following, select the applicable items, and click Apply.
    Device: CIFX 90E-RE\ET
    Channel Protocol: EtherCAT Master
  10. Select Firmware Download and click Browse.
  11. From the Firmware > CIFX folders, select the firmware file cifxecm.nxf. Click Open.
  12. Click Download.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.