EIO0000004200.07

Changing the UEFI BIOS Password

For security reasons, make sure you change the default password (Pw#12345). The following describes the procedure for changing the password.

NOTE: The password requires at least 3 characters.
  1. Display the BIOS screen. Refer to UEFI BIOS Setup Menu.
  2. Select Security.
  3. Select Administrator Password.
  4. The Enter Current password dialog box appears. Enter the current password.
  5. The Create New Password dialog box appears. Enter the new password.
  6. The Confirm New Password dialog box appears. Enter the same password as step 5.
  7. Press the [F4] key.
  8. Select Yes in the Save & Exit Setup dialog box.
  9. The product is restarted.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.