EIO0000004200.07

M.2 SSD Installation

The following describes how to install the M.2 SSD card. The size of the M.2 SSD card conforms to Type 2242. M.2 SSD becomes Disk 0.

When installing the M.2 SSD, the optional M.2 cooling kit is required. Purchase and install using the following steps.

M.2 cooling kit for Advanced Box: HMIYP6HSM2A*1
M.2 cooling kit for Standard Box: HMIYP6HSM2S

*1 If you use the Advanced Box with the FAN kit, the M.2 cooling kit is unnecessary.

M.2 Cooling Kit Package Contents

For Advanced Box:

For Standard Box:

  1. Heat sink pad (for bottom)

  2. Heat sink pad (for top)

  3. Heat sink

  4. Screws for heat sink

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
  • Remove all power from the device before removing any covers or elements of the system, and prior to installing or removing any accessories, hardware, or cables.
  • Unplug the power cable from both this product and the power supply prior to installing or removing the product.
  • Always use a properly rated voltage sensing device to confirm power is off where and when indicated.
  • Replace and secure all covers or elements of the system before applying power to this product.
  • Use only the specified voltage when operating this product. The DC model is designed to use 24 Vdc, and the AC model is designed to use 100 to 240 Vac. Always check whether your device is DC or AC powered before applying power.
Failure to follow these instructions will result in death or serious injury.
CAUTION
STORAGE DEVICE DAMAGE AND DATA LOSS
  • Remove all power before making any contact with an installed storage device.
  • Use only our optional storage devices for this product.
  • Make sure you regularly back up the data.
  • Confirm the storage device is correctly oriented before insertion.
  • Do not bend, drop, or strike the storage device.
  • Do not touch inside the storage device or its connectors.
  • Do not disassemble or modify the storage device.
  • Keep the storage device dry.
Failure to follow these instructions can result in injury or equipment damage.
NOTICE
ELECTROSTATIC DISCHARGE
Take the necessary protective measures against electrostatic discharge before attempting to remove the cover.
Failure to follow these instructions can result in equipment damage.
NOTICE
BROKEN ENCLOSURE
Do not exert more torque than the amount specified.
Failure to follow these instructions can result in equipment damage.
  1. Disconnect the power supply from the Box Module.
  2. Touch the housing or ground connection (not the power supply) to discharge any electrostatic charge from your body.
  3. Remove 5 screws of the maintenance hatch cover and slide the cover to remove.
  4. Peel off the protective film from the underside of the bottom heat sink pad, and place in the M.2 SSD card installation area. Also peel off the protective film from the top surface of the heat sink pad. When using the Advanced Box with the FAN kit, this step is unnecessary.
    1. Advanced Box

    2. Standard Box

  5. Remove the screw from the M.2 SSD card installation area on the product.
    NOTE: Using a Phillips screwdriver #1 is recommended.
    1. Advanced Box

    2. Standard Box

  6. As shown below, insert the M.2 SSD card diagonally, then push from above.
  7. Secure the M.2 SSD card with the screw removed in step 5.
    NOTE:
    • Using a Phillips screwdriver #1 is recommended.

    • The necessary torque is 0.2 N•m (1.77 lb-in).

  8. Peel off the protective film from the underside of the upper heat sink pad, and place the heat sink pad on the M.2 SSD card. Also peel off the protective film from the top surface of the heat sink pad. When using the Advanced Box with the FAN kit, this step is unnecessary.
  9. Put in the heat sink, and attach with screws.
    When using the Advanced Box with the FAN kit, this step is unnecessary.
    NOTE: The necessary torque is 0.3 N•m (2.7 lb-in).
    1. Advanced Box

    2. Standard Box

  10. Replace the maintenance hatch cover and tighten the screws.
    NOTE: The necessary torque is 0.3 N•m (2.7 lb-in).
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.