EIO0000004200.07

RAID Configuration Workflow

To configure RAID, use the following steps.
  1. Use Intel® OptaneTM Memory and Storage Management to change from AHCI mode to RAID mode. Refer to Changing to RAID Mode.
  2. To set the RAID level and volume, use one of the following tools: Pre-installed tools vary depending on your system version (OS Base). You can check the OS Base from the Launcher. Refer to System.

    OS Base 2.0 or later:
    Intel® OptaneTM Memory and Storage Management
    (Refer to RAID Configuration with Intel® OptaneTM Memory and Storage Management.)

    OS Base 1.0:
    Intel® Rapid Storage Technology
    (Refer to RAID Configuration with Intel® Rapid Storage Technology.)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.