EIO0000004200.07

Calibration

Calibrates the touch coordinates.

NOTE:
  • Do not calibrate using the Control Panel Tablet PC Settings > Adjustment. If touch panel calibration is required, use the calibration method shown here.

  • Before running calibration, in the Windows display settings set the [Scale and layout] to 100% for the associated display. You cannot calibrate properly using other scaling settings.

Calibration screen instructions are different between analog resistive film and projected capacitive (P-CAP) displays. Perform calibration as per the screen instructions.

Analog resistive film display

Projected capacitive display

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.