EIO0000004200.07

Starting the Launcher

The Launcher is a utility that you can set up to start programs and settings. The Launcher allows for convenient touch-screen operation by displaying icons for registered various settings.

You can start the Launcher from the shortcut icon on the desktop.

Launcher top screen

NOTE:
  • To customize the Launcher, refer to Edit.

  • Download the latest version of the Harmony P6 and Harmony FP6 Utility from the following URL to keep the Launcher up to date.
    www.se.com/ww/en/download

  • When the Launcher is already installed, it is overwritten. If you used Edit to customize the Launcher, customize again.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?