EIO0000004200.07

Changing to RAID Mode - Procedure

  1. After running SetupRST.exe, the following is displayed. Select Yes.
  2. Select Next.
  3. Select the I accept the terms in the License Agreement check box, then select Next.
  4. Select the Switch system SATA controller to Intel® RST Premium mode (Recommended) check box, then select Next.
  5. Select Next.
  6. Select the check box, and select Next.
  7. Select Restart to restart the product.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.