EIO0000004200.07

RAID Levels

This product supports RAID. Supported RAID levels are as follows.

RAID 0
RAID 1
RAID 5 (supported only on Advanced Box)

NOTE:
  • Hot swap is supported.

  • When configuring RAID 5, an optional storage device is required. Refer to Accessories.

WARNING
EXPLOSION HAZARD
Never attempt to perform hot swap in hazardous locations.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
CAUTION
RISK OF INJURY OR EQUIPMENT DAMAGE
Do not touch the electronic boards while energized.
Failure to follow these instructions can result in injury or equipment damage.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.