EIO0000004200.07

PCI/PCIe Card Installation

When using the Advanced Box with PCI/PCIe slots attached, you can install commercially available PCI add-on cards or PCI Express add-on cards (PCI/PCIe cards). You can install PCI/PCIe cards with the following configuration.

  Slot 1 Slot 2
PCI x 1 + PCIe x 1 PCI PCIe
PCIe x 2 PCIe1 PCIe2
PCI x 2 PCI1 PCI2
NOTE: The total power consumption of PCI/PCIe cards can be up to 12 W, regardless of whether one or two cards are installed.

PCI/PCIe card dimensions

The maximum size of PCI/PCIe cards that can be installed are as follows.

  1. PCI add-on card (short length)

  2. PCI Express add-on card (half length)

  3. I/O bracket

Installation procedure

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
  • Remove all power from the device before removing any covers or elements of the system, and prior to installing or removing any accessories, hardware, or cables.
  • Unplug the power cable from both this product and the power supply prior to installing or removing the product.
  • Always use a properly rated voltage sensing device to confirm power is off where and when indicated.
  • Replace and secure all covers or elements of the system before applying power to this product.
  • Use only the specified voltage when operating this product. The DC model is designed to use 24 Vdc, and the AC model is designed to use 100 to 240 Vac. Always check whether your device is DC or AC powered before applying power.
Failure to follow these instructions will result in death or serious injury.
NOTICE
ELECTROSTATIC DISCHARGE
Take the necessary protective measures against electrostatic discharge before attempting to remove the cover.
Failure to follow these instructions can result in equipment damage.
NOTICE
BROKEN ENCLOSURE
Do not exert more torque than the amount specified.
Failure to follow these instructions can result in equipment damage.
  1. Disconnect the power supply from the Box Module.
  2. Touch the housing or ground connection (not the power supply) to discharge any electrostatic charge from your body.
  3. Remove the screws (4 pieces) of the PCI/PCIe slot cover.
  4. Slide the cover in the direction of the arrow on the top of the cover, and remove it.
  5. Remove the screw from the interface cover, then remove the cover.
  6. Insert the PCI/PCIe card, and secure the card with the screw removed in step 5.
    NOTE: The necessary torque is 0.3 N•m (2.7 lb-in).
    1. PCI/PCIe card

  7. Replace the PCI/PCIe slot cover and tighten the screws.
    NOTE: The necessary torque is 0.3 N•m (2.7 lb-in).
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.