EIO0000004200.07

RS-232C isolated x 2

Specifications

  1. After attaching to the unit, right side

  2. After attaching to the unit, left side

Product number HMIYP6MPR23P2
Asynchronous transmission RS-232C (isolated) x 2
Data length 7 or 8 bits
Stop bit 1 or 2 bits
Parity None, odd or even
Data transmission speed 2,400...115,200 bps
Connector D-Sub 9 pin (plug)

The serial interface is isolated. The SG (signal ground) and FG (frame ground) terminals are not connected inside this product. When the serial interface connector is D-Sub, connect the FG wire to the shell.

DANGER
ELECTRIC SHOCK AND FIRE
When using the SG terminal to connect an external device to this product:
  • Verify that a ground loop is not created when you set up the system.
  • Connect the SG terminal to remote equipment when the external device is not isolated.
  • Connect the SG terminal to a known reliable ground connection to reduce the risk of damaging the circuit.
Failure to follow these instructions will result in death or serious injury.
CAUTION
LOSS OF COMMUNICATION
  • Do not put excessive stress on the communication ports of all connections.
  • Securely attach communication cables to the panel wall or cabinet.
  • Use a D-Sub 9 pin connector that has jack screws.
Failure to follow these instructions can result in injury or equipment damage.
NOTE: Use within the rated current.

Pin Assignment

D-Sub 9 pin plug connector

Module side:

Pin No. RS-232C
Signal name Direction Description
1 CD Input Carrier detect
2 RD (RXD) Input Receive data
3 SD (TXD) Output Send data
4 ER (DTR) Output Data terminal ready
5 SG - Signal ground (isolated)
6 DR (DSR) Input Data set ready
7 RS (RTS) Output Request to send
8 CS (CTS) Input Send possible
9 CI (RI) Input Called status display
Shell FG - Frame ground

Recommended jack screw is #4-40 (UNC).

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.