EIO0000004200.07

When using RS-485

To use auto direction control for RS-485, the port must be configured in the Windows® Device Manager.
  1. Open the Windows® Device Manager.
  2. Open Ports.
  3. Right-click the port that RS-485 is assigned to. Assigned ports vary depending on the configured optional interfaces. Refer to Before Using Serial Interface Options (the example below uses COM5 and COM6).
  4. Select Properties and open the Port Settings tab.
  5. Select the RS-485 check box.
  6. Turn Around Time specifies the length of time (data bit time) after transmission of communication data is complete, until the system changes to a state where it can receive communication data. After the specified time elapses, the system is in the state to receive data. Set the data bit time if used in a long-distance communication environment where propagation delay needs to be considered. The default value is 0.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.