EIO0000004200.07

Shell

You can hide the Windows® desktop by switching from the Explorer Shell to the Custom Shell. By doing so, you can suppress Windows® functions such as the Control Panel.

Custom Shell: The Windows® desktop is not displayed.
Explorer Shell: The Windows® desktop is displayed.

NOTE:
  • Install applications in the Explorer Shell.

  • When changing to the custom shell, the features shown in the Explorer Shell (such as Windows® desktop, Start menu, taskbar) cannot be used.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.