EIO0000004200.07

Interfaces

NOTE: Use only the SELV (Safety Extra-Low Voltage) circuit to connect all the interfaces.

Box Module

  Advanced Box / Standard Box
Serial interface COM Asynchronous transmission RS-232C (non-isolated) x 1
Data length 7 or 8 bits
Stop bit 1 or 2 bits
Parity None, odd or even
Data transmission speed 2,400...115,200 bps
Connector D-Sub 9–pin (plug)
USB (Type A) interface Connector USB 3.0 (Type A) x 2
USB 2.0 (Type A) x 2
Power supply voltage 5 Vdc ±5%
Maximum current supplied USB 3.0 (Type A): 900 mA/port
USB 2.0 (Type A): 500 mA/port
Maximum transmission distance USB 3.0 (Type A): 3 m (9.84 ft)
USB 2.0 (Type A): 5 m (16.4 ft)
USB (Type C) interface*1 Connector USB 3.0 (Type C) x 1
Power supply voltage 5 Vdc ±5% or 12 Vdc ±5%, USB power delivery (source) supported
Maximum current supplied 900 mA/port
3000 mA/port when USB power delivery is enabled*2 *3
Maximum transmission distance 3 m (9.84 ft)
Resolution Up to 4,096 x 2,304 pixels at 60 Hz
Ethernet interface Standard IEEE1588, 10 BASE-T/ 100 BASE-TX/ 1000BASE-T, Wake-on-LAN (WOL) supported*4
Connector Modular jack (RJ-45) x 2
DisplayPort Version V 1.2, dual mode (DP++) supported
Resolution Up to 4,096 x 2,304 pixels at 60 Hz

*1 The USB (Type C)interface supports alternate mode (DisplayPort) and USB power delivery (source, 5 Vdc/12 Vdc). When using USB power delivery, an E-Marked (electronically marked) cable is required.

*2 When Advanced Box is connected to the Display Module, the power supply capability of USB power delivery is limited to 30 W.

*3 For Standard Box, USB power delivery is effective only when Standard Box is used alone.

*4 When the status is S4 (hybrid shutdown), Wake-on-LAN is unavailable.

Display Module

  12-inch / 15-inch
USB (Type A) interface Connector USB 2.0 (Type A) x 1
Power supply voltage 5 Vdc ±5%
Maximum current supplied 500 mA
Maximum transmission distance 5 m (16.4 ft)
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.